Hello team ,
Do we have any documents relating to the performance of the length of the wire from the Ultrasonic sensor to the TDC1000 ,
My customer require at least 2~3 meter long wire because they are working for commercial vehicle. They will use shield cable in vehicle wiring harness.where they have placed the PCB with TDC.
The transducer are on the bottom of the tank stuck with ultrasonic glue . boost circuitry is on the chassis which around 2 meter away
The length of the wire is between the Transducer and TDC1000
( however we are using boost circuitry as shown in this EVM design http://www.ti.com/lit/ug/sniu026a/sniu026a.pdf )
So basically the distance between the transducer and the green board below
Can you please help me out in suggesting the architecture for interface if the tank is 2-3 Meter away from the main on board computer .
Also one more query from my end customer is regarding the glue .
Which glue is the suggested glue for transducer on a metal tank ?
This is will be in automotive application , hence can it be used in moisture , humidity hard environment condition
It will be exposed to lot of vibrations , also , will it be good in such condition ?
Thank you