Part Number: TDC1000-TDC7200EVM
1)
would like to shere the results that I had today
With the TDC1000-TDC7200EVM
I made today experiment of the water level
My target today was to see changes of positives numbers in the TOFAVG
While I am adding water to can
But instead of increasing number of the TOF AVG
I I've got results of decreasing numbers
The changes were very linear and stable
But in the opposite direction
Attached the config text
And short video that I made
Please your updates about the issue
2)
As a continues with my experiments on the EVM
I managed to get the rising of the numbers while I add water
And it made by changing in the
TIMEOUT(0X8) sector
FORCE_SHORT _TOF TO ENABLE in the TDC1000
But I think that the level of the water is not affect on the numbers
They increase in the start and then it stay there
No matter what is the water level
Please your advice
And also I've tried the config that sent to me by scott and it's not work and stuck the EVM
TDC1000_Config0 41 TDC1000_Config1 41 TDC1000_Config2 24 TDC1000_Config3 04 TDC1000_Config4 4A TDC1000_TOF-1 03 TDC1000_TOF-0 FF TDC1000_Error_Flags 00 TDC1000_Timeout 23 TDC1000_Clock_Rate 00 TDC1000_Conts_Trigger 01 TDC7200_Config1 02 TDC7200_Config2 40 TDC7200_Interrupt_Status 07 TDC7200_Interrupt_Mask 07 TDC7200_Coarse_Cntr_Ov_H FF TDC7200_Coarse_Cntr_Ov_L FF TDC7200_Clock_Cntr_Ov_H FF TDC7200_Clock_Cntr_Ov_L FF TDC7200_Clock_Cntr_Stop_Mask_H 00 TDC7200_Clock_Cntr_Stop_Mask_L 00 TRIGGER_UPDATE_FREQ 0000 TDC_AVG/STDEV_NUM_ELEMS 0032 SAVE_GRAPH_DATA_TO_FILE 00 FLOW_MODE_SELECT 00 Y-SCALE_CENTER 0032 X-SCALE_RANGE 0032 MEASURE_RTD1 00 SAVE_RESULT_REGR_TO_FILE 00 GRAPH_MULTI_STOPS 00 TDC_SELECT 00 TEMP_RTD_SELECT 00 TEMP_RTD_MODE 01 TEMP_AVG/STDEV_NUM_ELEMS 000A SAVE_TEMP_DATA 00 GRAPH_YMAX_DATA 00000000000067B6 GRAPH_YMIN_DATA 0000000000006752 TDC1000-HV_DRV_EN1 00 TDC1000-HV_DRV_EN2 00 HV_DRV_EN1_Period 001E HV_DRV_EN2_Period 001E ENABLE_POWER_CYCLE 00 CLK_FREQ_(1-16MHz) 8.000000 CLK_SOURCE_SEL 00 CPU_CLK_FREQ 05 CPU_CLK_EN 00 TDC1000-HV_BST_PWR_EN 00 HV_BST_PWR_EN_Period 0000 FWD2REV_FLOW_DELAY 0000 TDC1000-IMPE_MATCH_EN 00 ENABLE_UART_STREAM 00 ENABLE_MSP430TIMER_TDC 00