This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/MMWAVE-DEVPACK: Automatic Applications

Expert 1985 points

Part Number: MMWAVE-DEVPACK
Other Parts Discussed in Thread: AWR1642, AWR1243, IWR1642

Tool/software: Code Composer Studio

Hi,

Which series (AWR or IWR : 1443 or 1642) is suitable for this applications:?

- blind spot detection (BSD),  lane change assistant (LCA)

What is the update rate of range estimation and angle estimation in this applications[50 meter for detection of human and car] ?(Hz)

Which series (AWR or IWR : 1443 or 1642) is suitable for long range radar (LLR), automatic cruise control (ACC) and forward collision warning (FCW) [100-150 meter for human and car detection]?  What is the update rate?(Hz)

Thanks and best regards,

Amin