This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1243: AW1243 Performance indicators,

Part Number: AWR1243


How many AWR1243 can cascade.How much is the isolation between single chip TR; As well as the maximum modulation of time.How much is the linearity.

  • Hello Lei Wang,
    We will get back to you on the cascading query. Regarding the isolation , the Tx-RX isolation is better than 30dB from the device side. The synth linearity has a frequency error less than 0.01% in the settled period.
    I am not sure I understood the modulation time part of it. The chirp time is configurable by the user and would depend on the slope , sampling rate and number of samples. The only restriction is the total sweep bandwidth should be within 4Ghz.

    Regards,
    Vivek
  • Hello Lei,
    Number of AWR1243 devices that can be cascaded is a function of the synchronization signal's link budget(20GHz). These details would be published in an application note in a few weeks time.

    -Raghu