Hello team,
My customer uses our OPT3001, it is on a small board, and they put the board in a small box, the size of the box is very similar with a matchbox, there is a transparent window in front of the box, the size of the window is about 1cm*0.8cm.
If they put the board outside, the light is about 100 lux, but if they put the board in the small box, the read the light is about 50 lux, which is much lower. Do you have any suggestion how to improve the accuracy when put it in the box? Thanks
Regards,
Nanfang