Hello,
Please can you advise me back if AWR1243 can transmit 3 TX simultaneously (with less power per channel is accepted)?
Thanks in advance
KR
Shai Berman
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Please can you advise me back if AWR1243 can transmit 3 TX simultaneously (with less power per channel is accepted)?
Thanks in advance
KR
Shai Berman
Hi Shai,
AWR1243 does not allow more than two Transmit antenna's to be simultaneously. This ticket is assigned to an expert to provide you with more information regarding this.
Thank you,
Vaibhav
Shai,
The cascade design is still work in progress. The application note is not ready to be released yet.
I will update you with the available date later.
Regards,
Michelle
Hi Vaibhav & Shai:
I have the same question. Are the three transmit enable simultaneously something that is discouraged due to power consumption in AWR1243 ? i am assuming the silicon is capable of doing it.
I would think that since AWR1243 is the only cacadable option within the AWR series, the three simultaneous transmit brings out the true benefit to the max.
Additionally there is competitor chipset which have the similar
IF bandwidth, are cascadable and have the three transmits operate simultaneously. Will 3Tx be possible in AWR1243 ES 2.0 or higher ?
Best Regards,
RJ