Part Number: TDC1000-TDC7200EVM
I am unable to connect my GUI to the EVM, I have listed out my steps for attempting to read the EVM. I have read through the TDC7200 manual, read through many threads, and watched you tube videos to no avail. Would someone please help me connect my EVM to the GUI so I can begin utilizing the EVM for testing?
I open GUI.
Hold down the SW button on the EVM, plug in the EVM to the computer.
The bottom of the EVM shows Connect Failed! Check Hardware.
My device manager shows two HIDs, I check for the latest installed drivers and windows tells me the latest drivers have been installed.
I update the MSP430 firmware to TDC720xEVM-Firmware-v2.07, the download shows Done! and no device connected per the installation manual.
An amber light illuminates on the EVM and the HIDs disappear from the Device Manager and I receive the connect failed.
Please help.