This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1443BOOST: mmWave Sensor Raw Data Capture Using the TSW1400 Board

Part Number: IWR1443BOOST

Hello, i have the ES1.0 silicon-version and in the Radar Studio, I load the BSS, and then the MSS firmware.

BSS: c:\ti\mmwave_dfp_00.06.00.05\firmware\bss\ar12xx_bss.bin
MSS:c:\ti\mmwave_dfp_00.06.00.05\firmware\mss\binary\ar1xxx_mss.bin

The next step is "click the SPI Connect button" -> Unfortunately the "SPI Connectivity stays red" and the Radar Studio Software crashes. (DevPack board JP5 is o.k.)

Best regards

Metin