Hi,
There are a couple of questions that I need help.
1. It is my understanding that with AWR1243 the GPIO pins are configurable via the SPI interface from an external host. I was able to get a adc_valid signal out from the GPIO_0 with radar studio. I understand this includes register writes to some specific registers.
If we want to do this via embedded code or even lua shell in radar studio, I need to know what is the prescribed procedure for this.
I was not able to locate anything of this nature about GPIO in the documents I have so far - the AWR1xx_interface control document.
Can you please provide some documentation or guidance about how to set this up ? Is t
2. What are all the possible signals that can be configured to show up on the GPIO_0, GPIO_1 and GPIO_2 ?
I understand that ADC valid signal is possible through radar studio. If I want to bring out the frame start signal on the GPIO_x pin on the AWR1243BOOST, what would be the procedure for this ?
Thank you,
RJ