TI mmWave EVM use LP87524B for PMIC of the Radar, but the maximum input voltage is 5V. this PMIC seems specially for the mmWave application with Spread-Spectrum Mode and Phase Interleaving . Although it also has the AEC-Q100 but the problem is the Radar normally connect the power to the battery which is 12V and need to be in the range from 9V~16V. So does TI has any other PMIC that can be used?