Hi everyone,
I'm wondering if the mmWave technique is appropriate to measure the distance to a round surface which is displaceable along a defined axis.
The measuring range is up to ~20 cm. Is there a minimum distance?
The accuracy / resolution should be ~0.1mm or better
The measuring frequency should be ~100Hz
The average energy consumption should be not too high because the device is to be operated with lithium-ion batteries.
Is one of the mmWave sensors suitable for this and could you please suggest one?
Many thanks and kind regards,
Dominic