Part Number: TDC1000-TDC7200EVM
HI Scott
first I would like to thank you for your advise
we managed to identify the water level by the EVM
with linear increasing of the TOF while I added water to the can
now we would like to get forward and start the water flow metering with 45 degree
between the sensors on an iron pipe
the thickness of the walls in about 3 mm and with diameter of 3 inch and also 4 inch
the full pressure of the water is about 8 PSI
1- what are the recommended transducers
2- what is the recommended distance between the transducers
thx
Ari