Other Parts Discussed in Thread: AWR1443
Hi, I would like to understand how the Measurement Rate Scene Parameter is validated by the mmWave Sensing Estimator. It seems to share a relationship with the Active Frame Time, but does it rely also on other factors?
In an example I put together using the estimator, the Active Frame Time (ms) is 15.76. The Measurement Rate I selected is 32, which the tool says is too high. 32 frames would be a total of 504.32 ms, which is just over 50% duty cycle. The tool says that a measurement rate of 31 is acceptable, which is 488.56 ms. Is there some minimum inter-frame spacing that must be honored? Other constraints that I am not factoring in? Thanks.
Bill