This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE4490: SPI Initialize and communication problem

Part Number: AFE4490

Hi ,

                              I interface AFE4490 with freescale customised controller.SPI communication is not working .when i try to read from led control register by writing 1 value am getting zero as a result.I checked with mosi lines in logic analyzer the data what i have wriiten is displayed on mosi line and when i read back am getting zero on miso line.I will attach the screenshots now.I used mhz,8mhz for clockrate.I need to know the clock rate to use .I am using mode 0 for spi.read sequence is disable spi_readbit and write one value to register and enable spi_read bit and reading back the data.I ahve already posted question but  didnt get the response .It would be great if you resolve the issue at earliest.Thank     s in advance.