Other Parts Discussed in Thread: AWR1443
Hi,
I have a requirement as mentioned below, and I have calculated the following configuration.
System parameters are : Range Resolution: 40cm. Range Max: 10m. Velocity max: 500kmph. Velocity resolution: 1kmph
Chirp parameters that I calculated :
No of samples per chirp = 64
Sampling rate : 37.5 Msps
Total chirp time = idle time+ADC start time+ramp time+ramp excess time = 2+3.14+1.71+0 = 6.85us (I understand that I will get only 90% settling in the filters)
Slope = 92.78MHz/us
BW = 450MHz
I want to know whether the AWR1243 device can accept this configuration. A slight change in the values are fine to fit the parameters to the resolution of 1 LSB. Other than that I dont want to change much of the profile/chirp configuration.
I am asking this because, The mmwave sensing estimator is giving negative values for some parameters. I also dont have a TSW1400 board with me to initialize the radar studio tool to cross check my calculations.
On a side note, without TSW1400, is there any way to use radar studio tool to check the configuration, as I understand I can use it to configure the board without TSW1400.
Thanks.
Santhana Raj