This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP302: Internal circuit of OUT terminal(3pin)

Part Number: TMP302



Hi!

Please tell me a internal circuit of OUT terminal(3pin).

Does it have a surge protection diode of high side or another protection circuit built-in?
Is there a problem with using it as follows?

Vs(5pin) : 1.8V
OUT(3pin) : Pull-up to 3.3V by 10Kohm


Best Regards,
itabi