This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LDC1000: Linear sensing

Guru 16770 points

Part Number: LDC1000

Hi

I'm referring the following blog.

In my last blog post, Inductive Sensing: Linear position sensing (Part 1) , I demonstrated how to implement a linear position sensor using a triangular target and a spiral coil. While good resolution can…
By in Technical articles > Analog

I want to realize linearity sensing using LDC1000 with stretched coil.

Overview

Distance between target and coil : 2mm - 3mm

Target size : W 10mm / L 10mm

Target material : Iron or Zinc

Target displacement : Max 5mm

We have to sense target displacement (~ 5mm) linearly.

What kind of coil do you think it is the best choice?

And do you have design support tools for that?

BestRegards