Other Parts Discussed in Thread: AWR1642
Hi,
According to my measurement, the antenna transmission power of the REV A board is around 10dB lower than the REV E1 board with exactly the same mmw demo program flashed. I'm still using the SDK 0.8. Does that matter? I see on the new REV A board, two temperature sensors are added. Is it because I didn't configure those sensors correctly?
Thanks.