This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1443BOOST: vitalsign demo error at CLI

Part Number: IWR1443BOOST

I tried to run vitalsign demo with IWR1443BOOST (the device is 964D).

When click "START" below error message was shown at matlab CLI.

Starting UI for vital Signs Demo ....
Opening configuration file profile_2d_VitalSigns_20fps.cfg ...
Serial port(s) already open. Re-initializing...

comportnum_str =

COM24


comportnum_str =

COM25

Sending configuration to AR14xx profile_2d_VitalSigns_20fps.cfg ...
sensorStop
flushCfg
dfeDataOutputMode 1
channelCfg 15 1 0
adcCfg 2 1
adcbufCfg 0 1 0 1
profileCfg 0 77 7 6 57 0 0 70 1 100 2000 0 0 40
chirpCfg 0 0 0 0 0 0 0 1
frameCfg 0 0 2 0 50 1 0
guiMonitor 0 0 0 1
vitalSignsCfg 0.7 1.5 512 512
sensorStart

Error using vitalSigns_demo_gui (line 238)
Undefined function or variable 'rangeBinPhase'.

Error in vitalSignsDemo_GUI/StartPushed (line 88)


Error in appdesigner.internal.service.AppManagementService/tryCallback (line 207
)


Error in matlab.apps.AppBase>@(source,event)tryCallback(appdesigner.internal.ser
vice.AppManagementService.instance(),app,callback,requiresEventData,event)

Error using matlab.ui.control.internal.controller.ComponentController/executeUse
rCallback (line 262)
Error while evaluating Button PrivateButtonPushedFcn

Can you check what is the problem?

Best regards,

Hayden