Part Number: TDC1000-TDC7200EVM
I have a colleague using the TDC1000-TDC7200EVM with a pair of AudioWell transducers.
They are trying to measure fluid flow - when they rotate the tube to a horizontal position the GUI seems to lock up. Any reason why that is?
They have updated the S/W to version 2.01, so they should be up to the latest version.
Another question - when they export their data from the GUI to an Excel file ('Save Graph Data to...') - what units are the data in?
1st column: Start to Stop 1ToF, 2nd column: Start to Stop2 ToF, etc. to Stop5 ToF. Same question for the rest of the columns: What units are they in?
Also - is there a way to know where the data came from / how it was calculated (for those columns that are 'calculated' and not just raw data.
Thanks