Champs,
So I donloaded the v 1.9.2 of the Sensing Solutions EVM GUI; and when I plug in the LDC1314DIAL-EVM to my PC I see it get assinged a COM port with the gemneric name EVM on it in Device Manager, so I'm assuming it's working. However, when you launch Sensing Solutions EVM GUI; it says Not COnnected in the lower right; but I don't see anything remotely useful in configuring the tool as to which COM port to look at or how to make it conenct- can't do a FW upgrade either until it connects... whats the trick here? I'm assuning it's some QS guide... but the GUI doesn't come with one of these...