This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDC1000-TDC7200EVM: TDC1000-TDC7200EVM

Part Number: TDC1000-TDC7200EVM

Hello all,

Board is TDC1000-TDC7200EVM, sensor 1MHz.I need to measure fluid level. The sensor is glued on the bottom of the plastic tank, fluid is water and level of water is up to 20cm. Unfortunately, all my attempts to measure level were unsuccessful - level is always 2.18cm and do not changed with changing of water level. I do not see the difference with scope too. Probably there are incorrect settings, but i did not succeed to set the correct one. Online settings generator did not help me too.

Can anyone send me working settings for my case.Thanks in advance.

Best regards,

Peter

  • I've got the same issue. TOF remains the same on fluid level change. I'm using 1 MHz sensor and TDC1000-TDC7200EVM. I've tried with on board 8 MHz oscillator and with CPU clock the results are the similar - I have not any success.
  • Please refer to this application note that describes many of the register settings and key things to watch out for when using the TDC1000 to measure fluid level: www.ti.com/.../snaa270.pdf

    The app note is based on the TDC1000-C2000EVM, but is applicable to the TDC1000-TDC7200EVM as well.

    I am attaching some settings that should get you started as well. 

    TDC1000_Config0                         44
    TDC1000_Config1                         41
    TDC1000_Config2                         00
    TDC1000_Config3                         0C
    TDC1000_Config4                         00
    TDC1000_TOF-1                           40
    TDC1000_TOF-0                           00
    TDC1000_Error_Flags                     00
    TDC1000_Timeout                         1B
    TDC1000_Clock_Rate                      00
    TDC1000_Conts_Trigger                   00
    TDC7200_Config1                         00
    TDC7200_Config2                         00
    TDC7200_Interrupt_Status                00
    TDC7200_Interrupt_Mask                  00
    TDC7200_Coarse_Cntr_Ov_H                FF
    TDC7200_Coarse_Cntr_Ov_L                FF
    TDC7200_Clock_Cntr_Ov_H                 FF
    TDC7200_Clock_Cntr_Ov_L                 FF
    TDC7200_Clock_Cntr_Stop_Mask_H          00
    TDC7200_Clock_Cntr_Stop_Mask_L          00
    TRIGGER_UPDATE_FREQ                     0001
    TDC_AVG/STDEV_NUM_ELEMS                 000A
    SAVE_GRAPH_DATA_TO_FILE                 00
    FLOW_MODE_SELECT                        00
    Y-SCALE_CENTER                          0032
    X-SCALE_RANGE                           0032
    MEASURE_RTD1                            00
    SAVE_RESULT_REGR_TO_FILE                00
    GRAPH_MULTI_STOPS                       00
    TDC_SELECT                              00
    TEMP_RTD_SELECT                         00
    TEMP_RTD_MODE                           01
    TEMP_AVG/STDEV_NUM_ELEMS                000A
    SAVE_TEMP_DATA                          00
    GRAPH_YMAX_DATA                         00000000004C4B40
    GRAPH_YMIN_DATA                         0000000000030D40
    TDC1000-HV_DRV_EN1                      00
    TDC1000-HV_DRV_EN2                      00
    HV_DRV_EN1_Period                       001E
    HV_DRV_EN2_Period                       001E
    ENABLE_POWER_CYCLE                      00
    CLK_FREQ_(1-16MHz)                      8.000000
    CLK_SOURCE_SEL                          00
    CPU_CLK_FREQ                            05
    CPU_CLK_EN                              00
    TDC1000-HV_BST_PWR_EN                   00
    HV_BST_PWR_EN_Period                    0000
    FWD2REV_FLOW_DELAY                      0000
    TDC1000-IMPE_MATCH_EN                   00
    ENABLE_UART_STREAM                      00
    ENABLE_MSP430TIMER_TDC                  00

  • Hi Scott,

    Thank you very much for your help.
    I'm familiar with the application note snaa270, but was unable to find the proper configuration. Unfortunately, settings file "0160.TDC1000_Setup.txt" you sent to me did not make improvement too. Measured tank level now is 0 cm. regardless if there is water or not.

    Best Regards,
    Peter