Hello,
A thread on this topic (link) has been opened in the CCS forum which I believe is not solved. Importing the project in a fresh CCSv7.2 installation for desktop fails with the same error "Device-id 'IR1443' is not recognized"; same when importing the project in CCS Cloud.
Setting the "device" setting in the file vitalSigns_lab.projectspec to IWR1443 instead of IR1443 fixes the import issue. It seems there are further issues during the linking and the binary flash file generation steps though, due to a confusion between MMWAVE_SDK_DEVICE and MMWAVE_SDK_DEVICE_TYPE. I have attached a projectspec file that worked throughout the build in my environment. It would be good this file is double checked.
Thanks,
François.