Hello,
I had couple of questions regarding the clock signals and also the current consumption of the chip:
1) What is the purpose of the MCU_CLKOUT? If the MCU has its own oscillator, wouldn't the commands be synchronized through SPI clock and the data though LVDS clock?
2) How does the PMIC_CLK work? From my understanding, it's used to synchronize the switching of the PMIC with the chip. Is that correct?
3) How are the current values determined in Table 5-3? Are those the maximum current that can be drawn from the supply? VIN_13RF1 and VIN_13RF2 is listed as 2000mA but we didn't see anything close to that from our test. Is there a way to determine the maximum drawn current based on our settings?
Thank you,
Faiz