Hello,
1) I was wondering, what the acceptable loss, return loss, coupling and phase imbalance are if we split the 20 GHz LO signal?
2) From my understanding, the master low frequency sync out signal (SYNC_OUT) signal is fed into slave sync in signal (SYNC_IN). The SYNC_OUT signal is also used for the SOP signal for flashing.
2a) Do you see any issue if the master SYNC_OUT signal is used for SOP and then fed into a slave SYNC_IN signal?
2b) Does the SYNC_OUT signal have to be conditioned if it's driving more than one slave?
Thanks,
Faiz