This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/AWR1642: Question about Adv-Frame configuration

Part Number: AWR1642


Tool/software: Code Composer Studio

hi ! 

I don't have any idea about Awr1642's Adv-frame configuration.Can ti offer some code for that , or where can i find some information about the process?

present ,  I want to combine two sub-frame as one frame. each sub-frame has 32 unique chirp(32 chirp is just for test),so the final total frame has 64 chirp.i try to modificate the mmwave-demo offer by ti which the version is mmwave_sdk_01_00_00_05. please help me to check the process wether or not is right.

1), calling the function named MmwDemo_notifySensorStop(); stop the sensor

2) , populating the gMmwMssMCB struct as below(i just paste parts Code segment):

/**************************************************************************************************************/
/**************************************************************************************************************/

rlFrameCfg_t     frameCfg1;
rlFrameCfg_t     frameCfg2;
uint16_t         ChirpCnt = 0;


frameCfg->chirpStartIdx        = 0;
frameCfg->chirpEndIdx          = 31;
frameCfg->numLoops             = 1;
frameCfg->numFrames            = 0;
frameCfg->framePeriodicity     = 100 * 1000000 / 5;
frameCfg->triggerSelect        = 1; //Software API based triggering
frameCfg->frameTriggerDelay    = 0 * 1000000 / 5;


profileCfg1.profileId             = 0;
profileCfg1.startFreqConst        = (uint32_t) (77 * (1U << 26) / 3.6);
profileCfg1.idleTimeConst         = (uint32_t)((float)7 * 1000 / 10);
profileCfg1.adcStartTimeConst     = (uint32_t)((float)7 * 1000 / 10);
profileCfg1.rampEndTime           = (uint32_t)((float)58 * 1000 / 10);
profileCfg1.txOutPowerBackoffCode = 0;
profileCfg1.txPhaseShifter        = 0;
profileCfg1.freqSlopeConst        = (uint32_t)(0.1 * (1U << 26) / (3.6*1e3*900));//(uint32_t)(68 * (1U << 26) / (3.6*1e3*900)); //2^26 * 1e6/((3.6*1e9)*900)
profileCfg1.txStartTime           = (uint32_t)((float)1 * 1000 / 10);
profileCfg1.numAdcSamples         = 256;
profileCfg1.digOutSampleRate      = 5500;
profileCfg1.hpfCornerFreq1        = 0;
profileCfg1.hpfCornerFreq2        = 0;
profileCfg1.rxGain                = 30;


profileCfg2.profileId             = 1;
profileCfg2.startFreqConst        = (uint32_t) (78 * (1U << 26) / 3.6);
profileCfg2.idleTimeConst         = (uint32_t)((float)7 * 1000 / 10);
profileCfg2.adcStartTimeConst     = (uint32_t)((float)7 * 1000 / 10);
profileCfg2.rampEndTime           = (uint32_t)((float)58 * 1000 / 10);
profileCfg2.txOutPowerBackoffCode = 0;
profileCfg2.txPhaseShifter        = 0;
profileCfg2.freqSlopeConst        = (uint32_t)(0.1 * (1U << 26) / (3.6*1e3*900));//(uint32_t)(68 * (1U << 26) / (3.6*1e3*900)); //2^26 * 1e6/((3.6*1e9)*900)
profileCfg2.txStartTime           = (uint32_t)((float)1 * 1000 / 10);
profileCfg2.numAdcSamples         = 256;
profileCfg2.digOutSampleRate      = 5500;
profileCfg2.hpfCornerFreq1        = 0;
profileCfg2.hpfCornerFreq2        = 0;
profileCfg2.rxGain                = 30;


/*first  profile polution*/
for(ChirpCnt = 0 ; ChirpCnt < 32  ; ChirpCnt ++){
      /* Populate the chirp configuration: */
      chirpCfg.chirpStartIdx   = ChirpCnt ;
      chirpCfg.chirpEndIdx     = ChirpCnt ;
      chirpCfg.profileId       = 0;
      chirpCfg.startFreqVar    = (uint32_t)((((ChirpCnt)*10e6) * ((uint64_t)(1<<26))) / (3.6*1e9));
      chirpCfg.freqSlopeVar    = (int16_t)(0 * ((uint64_t)(1<<26))) / ((uint64_t)(3.6*1e9*900));
      chirpCfg.idleTimeVar     = (uint32_t)((float)0 * 1000 / 10);
      chirpCfg.adcStartTimeVar = (uint32_t)((float)0 * 1000 / 10);
      chirpCfg.txEnable        = 1;
       /* Get the profile handle to which the chirp is to be added: */
      if (MMWave_getProfileHandle (gMmwMssMCB.ctrlHandle, chirpCfg.profileId,
                                   &profileHandle, &errCode) < 0)
      {
          /* Error: Unable to get the profile handle. Return the error code */
          return errCode;
      }

      /* Add the chirp to the profile */
      if (MMWave_addChirp (profileHandle, &chirpCfg, &errCode) == NULL)
      {
          /* Error: Unable to add the chirp. Return the error code. */
          return errCode;
      }
}

/*secend  profile polution*/
for(ChirpCnt = 0 ; ChirpCnt < 32  ; ChirpCnt ++){
      /* Populate the chirp configuration: */
      chirpCfg.chirpStartIdx   = ChirpCnt ;
      chirpCfg.chirpEndIdx     = ChirpCnt ;
      chirpCfg.profileId       = 1;
      chirpCfg.startFreqVar    = (uint32_t)((((ChirpCnt)*10e6) * ((uint64_t)(1<<26))) / (3.6*1e9));
      chirpCfg.freqSlopeVar    = (int16_t)(0 * ((uint64_t)(1<<26))) / ((uint64_t)(3.6*1e9*900));
      chirpCfg.idleTimeVar     = (uint32_t)((float)0 * 1000 / 10);
      chirpCfg.adcStartTimeVar = (uint32_t)((float)0 * 1000 / 10);
      chirpCfg.txEnable        = 1;
       /* Get the profile handle to which the chirp is to be added: */
      if (MMWave_getProfileHandle (gMmwMssMCB.ctrlHandle, chirpCfg.profileId,
                                   &profileHandle, &errCode) < 0)
      {
          /* Error: Unable to get the profile handle. Return the error code */
          return errCode;
      }

      /* Add the chirp to the profile */
      if (MMWave_addChirp (profileHandle, &chirpCfg, &errCode) == NULL)
      {
          /* Error: Unable to add the chirp. Return the error code. */
          return errCode;
      }
}


 /**************************************************************************************************************/
 /**************************************************************************************************************/


3) configuration the adv-frame struct
//******************************************************************************************************//
//******************************************************************************************************//
//this part of code is reference by :"\mmwave_sdk_01_00_00_05\mmwave_sdk_01_00_00_05\packages\ti\control\mmwavelink\test\common\testlink.c" 

rlAdvFrameCfg_t advFrameCfg;

memset(advFrameCfg , 0 , sizeof(advFrameCfg));

advFrameCfg.frameSeq.numOfSubFrames = 2,                                     // i wanna two subframe combine as one frame      
advFrameCfg.frameSeq.forceProfile = xxQ1,                                         //i have two profile , profile0 and profile1 but i don't kown what values should be set   in here  
advFrameCfg.frameSeq.reserved1 = 0,        
advFrameCfg.frameSeq.subFrameCfg[0].forceProfileIdx = 0, // mine first profile0          
advFrameCfg.frameSeq.subFrameCfg[0].chirpStartIdx = 0,   // start idx is 0 , and mine chirp is 0 - 31;          
advFrameCfg.frameSeq.subFrameCfg[0].numOfChirps = 32,    //               
advFrameCfg.frameSeq.subFrameCfg[0].numLoops = 0,        //          
advFrameCfg.frameSeq.subFrameCfg[0].burstPeriodicity = 0,// can it be 0 , after all i don't have burst          
advFrameCfg.frameSeq.subFrameCfg[0].chirpStartIdxOffset = xxQ2, // I don't follow this?       
advFrameCfg.frameSeq.subFrameCfg[0].numOfBurst = 1,                
advFrameCfg.frameSeq.subFrameCfg[0].numOfBurstLoops = 1,           
advFrameCfg.frameSeq.subFrameCfg[0].reserved1 = 0,                 
advFrameCfg.frameSeq.subFrameCfg[0].subFramePeriodicity = 0,// can it be zero      
advFrameCfg.frameSeq.subFrameCfg[0].reserved2 = 0,                
advFrameCfg.frameSeq.subFrameCfg[0].reserved3 = 0,

advFrameCfg.frameSeq.subFrameCfg[1].forceProfileIdx = 1,          
advFrameCfg.frameSeq.subFrameCfg[1].chirpStartIdx = 0,             
advFrameCfg.frameSeq.subFrameCfg[1].numOfChirps = 32,              
advFrameCfg.frameSeq.subFrameCfg[1].numLoops = 0,                 
advFrameCfg.frameSeq.subFrameCfg[1].burstPeriodicity = 0,          
advFrameCfg.frameSeq.subFrameCfg[1].chirpStartIdxOffset = 0,      
advFrameCfg.frameSeq.subFrameCfg[1].numOfBurst = 1,                
advFrameCfg.frameSeq.subFrameCfg[1].numOfBurstLoops = 1,           
advFrameCfg.frameSeq.subFrameCfg[1].reserved1 = 0,                 
advFrameCfg.frameSeq.subFrameCfg[1].subFramePeriodicity = 0,       
advFrameCfg.frameSeq.subFrameCfg[1].reserved2 = 0,                 
advFrameCfg.frameSeq.subFrameCfg[1].reserved3 = 0,     
           
advFrameCfg.frameSeq.numFrames = 0,         //infinite frames to transmit
advFrameCfg.frameSeq.triggerSelect = 1,     
advFrameCfg.frameSeq.frameTrigDelay = 0,    // can it be zero 
advFrameCfg.frameSeq.reserved2 = 0,                 

advFrameCfg.frameData.numSubFrames = 2,     //two sub-frame                 
advFrameCfg.frameData.reserved1 = 0,                  
advFrameCfg.frameData.reserved2 = 0,                  
advFrameCfg.frameData.subframeDataCfg[0].totalChirps = 32,  //numOfChirps * numLoops * numOfBurst = 32*1*1 = 32            
advFrameCfg.frameData.subframeDataCfg[0].numAdcSamples = 128, //64point * 2 = 128              
advFrameCfg.frameData.subframeDataCfg[0].numChirpsInDataPacket = 1,     
advFrameCfg.frameData.subframeDataCfg[0].reserved1 = 0,                
advFrameCfg.frameData.subframeDataCfg[1].totalChirps = 32,             
advFrameCfg.frameData.subframeDataCfg[1].numAdcSamples = 128,              
advFrameCfg.frameData.subframeDataCfg[1].numChirpsInDataPacket = 1,    
advFrameCfg.frameData.subframeDataCfg[1].reserved1 = 0,                

//******************************************************************************************************//
//******************************************************************************************************//

i have some problem about the code ,

Q1 : advFrameCfg.frameSeq.forceProfile;

what value should be set and what is means?
what the different between the advFrameCfg.frameSeq.forceProfile and advFrameCfg.frameSeq.subFrameCfg[1].forceProfileIdx?

Q2 : can advFrameCfg.frameSeq.subFrameCfg[0].burstPeriodicity be zeros?

Q3 : have some problem with the configration about advFrameCfg ?



4) calling the function MmwDemo_mssDataPathConfig() to configurated all of parameter to BSS

5) calling the function named MMWave_fullConfig() ;

//**********************************************************************************************************************//
//**********************************************************************************************************************//

static int32_t MMWave_fullConfig (MMWave_MCB* ptrMMWaveMCB, MMWave_CtrlCfg* ptrControlCfg, int32_t* errCode)
{
    int32_t             retVal = -1;
    MMWave_InitRFCfg    initRFCfg;

    /* Initialize the RF configuration: */
    memset ((void*)&initRFCfg, 0, sizeof(MMWave_InitRFCfg));

    /* Populate the configuration */
    initRFCfg.ptrChannelCfg      = &ptrControlCfg->u.fullControlCfg.chCfg;
    initRFCfg.ptrADCOutCfg       = &ptrControlCfg->u.fullControlCfg.adcOutCfg;
    initRFCfg.ptrLowPowerModeCfg = &ptrControlCfg->u.fullControlCfg.lowPowerMode;
    initRFCfg.freqLimitLow       = ptrControlCfg->freqLimitLow;
    initRFCfg.freqLimitHigh      = ptrControlCfg->freqLimitHigh;

    /* Initialize the RF: */
    retVal = MMWave_initRF (ptrMMWaveMCB, &initRFCfg, errCode);
    if (retVal < 0)
    {
        /* Error: Initialization of the RF failed; error code is already setup */
        goto exit;
    }

    /* Configure the Link with the application supplied configuration: */
    retVal = MMWave_configLink (ptrMMWaveMCB, ptrControlCfg, errCode);
    if (retVal < 0)
    {
        /* Error: Configuration of the Link failed; error code is already setup */
        goto exit;
    }

    /* Link configuration validated: We can now pass this to the SOC Handler. */
    retVal = gMMWaveHwAttributes.cfgFxn (ptrMMWaveMCB, ptrControlCfg, errCode);
    if (retVal < 0)
    {
        /* Error: mmWave Link configuration failed. Error code is already configured
         * Fall through! */
        goto exit;
    }

    
    /* mmWave Link configured. */
    ptrMMWaveMCB->isConfigured = true;


    /* Setup the return value: */
    retVal = 0;

exit:
    return retVal;
}

//**********************************************************************************************************************//
//**********************************************************************************************************************//

Q5 : i think i should add the function named:

rlSetAdvFrameConfig(RL_DEVICE_MAP_INTERNAL_BSS, (rlAdvFrameCfg_t*)&advFrameCfg);

into the function MMWave_configLink (ptrMMWaveMCB, ptrControlCfg, errCode), but i'm not sure where to add. I'v try to code it ,please help me check it :

6) add the function rlSetAdvFrameConfig(RL_DEVICE_MAP_INTERNAL_BSS, (rlAdvFrameCfg_t*)&advFrameCfg) into MMWave_configLink().

 

//**********************************************************************************************//
//**********************************************************************************************//
int32_t MMWave_configLink
(
    MMWave_MCB*         ptrMMWaveMCB,
    MMWave_CtrlCfg*     ptrControlCfg,
    int32_t*            errCode
)
{
    int32_t                 retVal;
    int32_t                 index;
    rlContModeEn_t          contModeEnable;
    rlProfileCfg_t          profileCfg;
    MMWave_ChirpHandle      chirpHandle;
    rlChirpCfg_t            chirpCfg;
    uint32_t                numChirps;
    uint32_t                chirpIndex;

    /* Determine the DFE Output mode? */
    if (ptrControlCfg->u.fullControlCfg.dfeDataOutputMode == MMWave_DFEDataOutputMode_CHIRP)
    {
        /**************************************************************************
         * Chirp Mode:
         * Order of operations as specified by the mmWave Link are
         *  - Profile configuration
         *  - Chirp configuration
         *  - Frame configuration
         **************************************************************************/
        for (index = 0; index < MMWAVE_MAX_PROFILE; index++)
        {
            /* Do we have a valid profile? */
            if (ptrControlCfg->u.fullControlCfg.u.chirpModeCfg.profileHandle[index] == NULL)
            {
                /* NO: Skip to the next profile */
                continue;
            }

            /* YES: Get the profile configuration */
            if (MMWave_getProfileCfg (ptrControlCfg->u.fullControlCfg.u.chirpModeCfg.profileHandle[index],
                                      &profileCfg, errCode) < 0)
            {
                /* Error: Unable to get the profile configuration. Setup the return value */
                retVal = -1;
                goto end;
            }

            /* Configure the profile using the mmWave Link API */
            retVal = rlSetProfileConfig (RL_DEVICE_MAP_INTERNAL_BSS, 1U, &profileCfg);
            if (retVal != RL_RET_CODE_OK)
            {
                /* Error: Setting the profile configuration failed */
                *errCode = MMWAVE_EPROFILECFG;
				MMWave_translateErrorCode(&retVal);
                goto end;
            }

            /* Get the number of chirps configured and attached to the profile: */
            if (MMWave_getNumChirps (ptrControlCfg->u.fullControlCfg.u.chirpModeCfg.profileHandle[index],
                                     &numChirps, errCode) < 0)
            {
                /* Error: Unable to get the number of chirps. Error code is already setup */
                retVal = -1;
                goto end;
            }

            /* For the profile; Cycle through all the chirps and configure them. */
            for (chirpIndex = 1U; chirpIndex <= numChirps; chirpIndex++)
            {
                /* Get the Chirp Handle associated at the specified index */
                if (MMWave_getChirpHandle (ptrControlCfg->u.fullControlCfg.u.chirpModeCfg.profileHandle[index],
                                           chirpIndex, &chirpHandle, errCode) < 0)
                {
                    /* Error: Unable to get the chirp handle. Error code is already setup */
                    retVal = -1;
                    goto end;
                }

                /* Get the chirp configuration: */
                if (MMWave_getChirpCfg (chirpHandle, &chirpCfg, errCode) < 0)
                {
                    /* Error: Unable to get the chirp configuration. Error code is already setup */
                    retVal = -1;
                    goto end;
                }

                /* Set the chirp configuration in the mmWave link */
                retVal = rlSetChirpConfig(RL_DEVICE_MAP_INTERNAL_BSS, 1U, &chirpCfg);
                if (retVal != RL_RET_CODE_OK)
                {
                    /* Error: Setting the chirp configuration failed */
                    *errCode = MMWAVE_ECHIRPCFG;
					MMWave_translateErrorCode(&retVal);
                    goto end;
                }
            }
        }

        /* Set the frame configuration: */
        //retVal = rlSetFrameConfig(RL_DEVICE_MAP_INTERNAL_BSS, &ptrControlCfg->u.fullControlCfg.u.chirpModeCfg.frameCfg);
          retVal = rlSetAdvFrameConfig(RL_DEVICE_MAP_INTERNAL_BSS, (rlAdvFrameCfg_t*)&advFrameCfg);if (retVal != RL_RET_CODE_OK)
        {
            /* Error: Setting the frame configuration failed */
            *errCode = MMWAVE_EFRAMECFG;
			MMWave_translateErrorCode(&retVal);
            goto end;
        }
    }
    else
    {
        /**************************************************************************
         * Continuous Mode:
         * Order of operations as specified by the mmWave Link are
         *  - Continuous Mode configuration
         *  - Device enable streaming
         **************************************************************************/
        retVal = rlSetContModeConfig (RL_DEVICE_MAP_INTERNAL_BSS, &ptrControlCfg->u.fullControlCfg.u.continuousModeCfg.contModeCfg);
        if (retVal != RL_RET_CODE_OK)
        {
            *errCode = MMWAVE_ECONTMODECFG;
			MMWave_translateErrorCode(&retVal);
            goto end;
        }

        /* Initialize the continuous mode configuration: */
        memset ((void*)&contModeEnable, 0, sizeof(rlContModeEn_t));

        /* Populate the continuous mode configuration: */
        contModeEnable.contModeEn = 1U;
        retVal = rlEnableContMode (RL_DEVICE_MAP_INTERNAL_BSS, &contModeEnable);
        if (retVal != RL_RET_CODE_OK)
        {
            *errCode = MMWAVE_ECONTMODE;
			MMWave_translateErrorCode(&retVal);
            goto end;
        }
    }

    /* Set the return value to be success. */
    retVal = 0;

end:
    return retVal;
}

//**********************************************************************************************//
//**********************************************************************************************//

i just used the function

retVal = rlSetAdvFrameConfig(RL_DEVICE_MAP_INTERNAL_BSS, (rlAdvFrameCfg_t*)&advFrameCfg);

instead of the function
retVal = rlSetFrameConfig(RL_DEVICE_MAP_INTERNAL_BSS, &ptrControlCfg->u.fullControlCfg.u.chirpModeCfg.frameCfg);

can it be work?otherwise how can i do it?


BR
havi

  • Hello Havi,

    mmWave Link API calls are explained in the Doxygen html file which are part of SDK installation. Wanted to make sure you have looked at these helpful html files already.

     Following is the typical path under mmWaveSDK installation dir:

    mmWaveLink Framework: file:///C:/ti/mmwave_sdk_01_00_00_05/packages/ti/control/mmwavelink/docs/doxygen/html/index.html

    Above html give overview of the mmWaveLInk.  You would want to check the following hierachy from the above page

    mmWaveLink Framework

    |--Modules

    |--Sensor

    This should take you to the following page (typically) :  file:///C:/ti/mmwave_sdk_01_00_00_05/packages/ti/control/mmwavelink/docs/doxygen/html/group___sensor.html

    Above page should show various (RF) sensor related API calls,  the one for Advanced Frame Config is :  "rlSetAdvFrameConfig"

    Clicking on the function will show the description and Structure of container "rlAdvFrameCfg_t ",  clicking here will take you to two data structures in this container.

    rlAdvFrameSeqCfg_t  frameSeq : file:///C:/ti/mmwave_sdk_01_00_00_05/packages/ti/control/mmwavelink/docs/doxygen/html/structrl_adv_frame_seq_cfg__t.html
     
    rlAdvFrameDataCfg_t  frameData : file:///C:/ti/mmwave_sdk_01_00_00_05/packages/ti/control/mmwavelink/docs/doxygen/html/structrl_adv_frame_data_cfg__t.html

    Various fields of these fields are explained under each data struct.

    Hope this helps.

    Thank you,

    Vaibhav

  • Hello Vaibhav

    thank you.

    i'm trying , but when i Populated the register : advframecfg->frameSeq.subFrameCfg[0].forceProfileIdx;

    the doc says :

    "rlUInt16_t rlSubFrameCfg_t::forceProfileIdx

    Force profile index. This is applicable only if FORCE_SINGLE_PROFILE is set to 1"

    i can not find where the FORCE_SINGLE_PROFILE 's definition.

    is this "FORCE_SINGLE_PROFILE " means the register named advframecfg->frameSeq.forceProfile = 0x01 ?

    thank you ,

    Havi
  • Hello Havi,

    forceProfileIdx is applicable only if forceProfile is set to '1'. 

     rlSubFrameCfg_t::forceProfile

    value definition
    0x0 The profile index set in Chirp Config API message governs which profile is used when that chirp is transmitted
    0x1 The profile index indicated in Chirp Config message is ignored and all the chirps in each sub frame use a single profile as indicated by that sub frame’s profile index set in this message.



    For details info about rlAdvFrameCfg_t parameters of rlSetAdvFrameConfig API  please refer Radar Interface control document which is available in mmWave-dfp package.

    Here you find the literature of advanced frame configuration.

    Hope these two document will clarify your queries.

    Regards,

    Jitendra Gupta