Hi Team,
One of our customer has evaluated and like to use our FDC2214 for the liquid-level detect solution. They need some cost down to meet target solution cost hence looking at alternate source for the inductor and the oscillator.
Kindly advise what are the key specifications need to consider selecting the inductor and the oscillator for FDC2214 circuit. With reference to the device used in the EVM such as CMH322522-180KL and CTS's 625L3C040M.
For the 18uH inductor, can we use 25mA for Irms-max since FDC2214 output drive is in the range of 1.5mA to 6mA (max) ?
DS stated inductor SRF must > 125% of sensor LC frequency.
What is the low limit for the Q-factor ?
What is the maximum inductor DCR that FDC2214 can drive ?
For the 40MHz oscillator, what are the key specification that must be met ?
Frequency stability +/-50ppm ? Aging < +/-5ppm/yr.
can we use higher supply current >15mA device ?
Can you provide some calculation example relating the +/10% tolerance of the inductor to FDC2214's ADC output resolution accuracy ? Similarly the oscillator's frequency stability to FDC2214 output ENOB.
Look forward to your feedback, thanks in advance.