Looking at the list of subsystems that can be calibrated on the AW1243 under the RF_INIT_CALIB_ ENABLE_MASK, is there a description somewhere for each describing the validity of the calibration? For example in my past experience calibration executed at power up is good as long as device temperature had not risen more than 5 degree C. Once the temperature had changed the calibration was no longer considered valid and needed to be re-executed. For this device, of the following calibration options when is the calibration no longer valid and need to be re-executed?
Bit Definition
4 Enable LODIST calibration
5 Enable RX ADC DC offset calibration
6 Enable HPF cutoff calibration
7 Enable LPF cutoff calibration
8 Enable Peak detector calibration
9 Enable TX power calibration
10 Enable RX gain calibration
11 Enable TX Phase calibration
12 Enable RX IQMM calibration