This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LDC1312: Where is the electrical spec for INTB output?

Part Number: LDC1312

The LDC1312/1314 datasheet seems to be missing the electrical table specification for the INTB output.   The I2C specification is there but no mention of INTB.  It's not clear whether the output is open drain or totem-pole, and what the Voh Vol are at test currents.  The simple diagram Figure 54 shows no pullup resistor on INTB, implying totem-pole, but the I2C are drawn without pullups either so I can't tell what assumptions are made.  There is no pullup on the eval board that I can see on schematic, but maybe the MCU internal IO pullup is used.  Can you please clarify the electrical parameters of this port?