This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1243BOOST: Maximum power comsumption at AWR1243BOOST.

Part Number: AWR1243BOOST
Other Parts Discussed in Thread: TPS7A88

Regarding power consumption. About RF input of 1.3V , document describes maximum 2000 mA.

AWR1243Boosts EVM has TPS7A88 that the current limit of LDO is 1.5 - 1.9A.

(1) What kind of conditions were used when the maximum power consumption was calculated.

(2) I would like to know if there are any cases that EVM cannot work by LDO maximum current limit.

Best Regards

KORO