1. Is it necessary to issue a line from the E14 terminal and the D13 terminal in the circuit diagram of AWR 1642 BOOST in order to communicate using CAN? Or, can I assign N4, N5 to CAN?
2. Can TI provide software that communicates via CAN?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1. Is it necessary to issue a line from the E14 terminal and the D13 terminal in the circuit diagram of AWR 1642 BOOST in order to communicate using CAN? Or, can I assign N4, N5 to CAN?
2. Can TI provide software that communicates via CAN?
Vivek san
According to the AWR1642 datasheet , N4 and N5(default RS232 function) are able to be assigned CAN-FD.
But I can't find how to assign the PIN function.
Could you tell me which doucument explain this ?
Best Regards,.
Vivek san
Thank you very much.
I was able to find the setting part.
I'm looking forward that SDK will be released with support for CAN communication.
Best regards,.