This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1642BOOST: Is USB connector of the IWR1642BOOST brocken?

Part Number: IWR1642BOOST

When IWR1642BOOST connect with 5V input, red led of the board is brighten.

However, when IWR1642BOOST connect to computer with USB connector, red led of the board is not brighten, and device manager of the computer is not show up this device.

Is USB connector of the IWR1642BOOST brocken?