Hi,
We are evaluating DDC114 and I am seeing some strange behaviour.
I am running the simplest config possible with a continuous 250Hz CONV (2ms Tint) , 4MHz CLK and trigger off DVALID to get 80bits of data while TEST is held high
I see that the first 2 values recieved (Inputs 4 and 3) are around 3000 counts (so slightly negative) while the next 2 (inputs 2 and 1) are around 4000 which seems more normal (around 0% full-scale). This 1000 negative offset is present when I leave Test mode and measure actual input currents.
My question is what is the expected value in a well designed PCB during Test mode and what can cause that offset on only 2 channels?
Thanks,
Petros