Hi,
My customer face one issue that the profile reconfiguration doesn't take effect. They call the rlSetProfileConfig to reconfigure the profile per frame without sensor stop and restart, they can guarantee the profile reconfiguration completion before next frame start. They use the spectrum analyzer to measure the IF signal from mixer, but find the signal doesn't change along with the profile reconfiguration.
Before they have tested chirp reconfiguration through calling rlSetChirpConfig also without sensor stop and restart, also using the same method to measure the IF signal which can change well along with the chirp reconfiguration.
So would u pls help check whether the profile can be reconfigured in this way? The test is based on mmw demo in sdk 1.0.
Thanks & BR,
Andy