Part Number: AWR1443BOOST
Other Parts Discussed in Thread: AWR1443, , MMWAVE-SDK
Tool/software: Code Composer Studio
Hi,
I'm trying to start an mmWave project on CCS using mmWave link. I've included the mmwavelink.h header file and a few standard C librabries. Im following your mmWave radar programming model video and have just wrote a few lines to test mmwave link. However, whenever i try to debug my code i get an error saying:
Description Resource Path Location Type
mklib: gmake error during rtsv7R4_A_le_v3D16_eabi.lib build mklib: gmake error during rtsv7R4_A_le_v3D16_eabi.lib build mmWave C/C++ Problem
Debugging also forces my CPU to 100% CPU usage and takes a very long time. Any help would be appreciated.
Here's my starting code:
#include <C:/ti/mmwave_sdk_01_00_00_05/packages/ti/control/mmwavelink/mmwavelink.h>
#include <stdint.h>
#include <stdlib.h>
#include <stddef.h>
#include <string.h>
#include <stdio.h>
#include <math.h>
/**
* main.c
*/
int main(void)
{
rlProfileCfg_t profCfg;
profCfg.profileId = 0;
profCfg.startFreqConst = 0x558E38E3;
}
Thanks