This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

FDC1004EVM: EVM GUI Source Code?

Part Number: FDC1004EVM

Hello, I'm looking for a link to software libraries that would support using the USB interface to the FDC1004EVM; is this available?  The source code of the EVM GUI should be sufficient.

  • Hi Tom Hanks3,

    You can refer to the SensingSolutionsEvm_Protocol_0v1 java script file for USB communication protocol between the GUI and the EVM. The file is located under PC GUI\node_modules\SspEvmNodeJS in the Sensing Solutions EVM GUI installation folder.

    Please make sure you update to the latest firmware located in the GUI installation folder.

    Regards,

    Varn.