This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/TMP75: temperature sensor porting confer (Android OS)

Part Number: TMP75

Tool/software: Linux

Hi 

excuse me, recently I try to porting tmp75 into Android OS, some of information as below

OS: android 6.0.1

linux version: 4.1.15

the first step probe driver already finished, and the power gpio was set finished, but when enter to system, the log as below 

and the attachment file is my tmp75 driver (lm75.c / lm75.h)

could any one help me to check why the  "thermal_zone_of_sensor_register()" could get error (the red number [ 4.772457] data->tz is -19 )

4.675158] **********enter dm5150_switch_AUX(cvbs)
[ 4.680067] **********cvbs is 1
[ 4.683687] dm5150 CVBSin1 (Mux0)
[ 4.687127] ***********enter dm5150_get_std in dm5150_switch_AUX()
[ 4.693935] tmp is 0
[ 4.696133] Got invalid video standard!
[ 4.707995] VD_MISC : 0x06
[ 4.710725] ********in ioctl_g_fmt_cap
[ 4.715854] mxc_v4l2_output v4l2_out: V4L2 device registered as video16
[ 4.722700] mxc_v4l2_output v4l2_out: V4L2 device registered as video17
[ 4.729755] usbcore: registered new interface driver uvcvideo
[ 4.735516] USB Video Class driver (1.1.1)
[ 4.740640] **********************add lm75 driver*********************
[ 4.747357] ******start probe tmp75******
[ 4.751382] in probe switch******
[ 4.754707] kind is 19
[ 4.757101] choose tmp75
[ 4.759645] ********in lm75_read_value
[ 4.763402] 1
[ 4.765620] ********probe status is 0
[ 4.769793] Config 0x60
[ 4.772457] data->tz is -19
[ 4.775264] data->tz is error******
[ 4.778792] 8??5%?
[ 4.782207] imx2-wdt 20bc000.wdog: timeout 60 sec (nowayout=0)
[ 4.788660] device-mapper: uevent: version 1.0.3
[ 4.793701] device-mapper: ioctl: 4.31.0-ioctl (2015-3-12) initialised: dm-devel@redhat.com
[ 4.802263] Bluetooth: HCI UART driver ver 2.3
[ 4.806746] Bluetooth: HCI UART protocol H4 registered
[ 4.811897] Bluetooth: HCI UART protocol BCSP registered
[ 4.817243] Bluetooth: HCI UART protocol ATH3K registered
[ 4.822768] usbcore: registered new interface driver btusb
[ 4.828502] sdhci: Secure Digital Host Controller Interface driver
[ 4.834700] sdhci: Copyright(c) Pierre Ossman

REALLY THX

/*
 * lm75.c - Part of lm_sensors, Linux kernel modules for hardware
 *	 monitoring
 * Copyright (c) 1998, 1999  Frodo Looijaard <frodol@dds.nl>
 *
 * This program is free software; you can redistribute it and/or modify
 * it under the terms of the GNU General Public License as published by
 * the Free Software Foundation; either version 2 of the License, or
 * (at your option) any later version.
 *
 * This program is distributed in the hope that it will be useful,
 * but WITHOUT ANY WARRANTY; without even the implied warranty of
 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
 * GNU General Public License for more details.
 *
 * You should have received a copy of the GNU General Public License
 * along with this program; if not, write to the Free Software
 * Foundation, Inc., 675 Mass Ave, Cambridge, MA 02139, USA.
 */

#include <linux/module.h>
#include <linux/init.h>
#include <linux/slab.h>
#include <linux/jiffies.h>
#include <linux/i2c.h>
#include <linux/hwmon.h>
#include <linux/hwmon-sysfs.h>
#include <linux/err.h>
#include <linux/mutex.h>
#include <linux/of_device.h>
#include <linux/of.h>
#include <linux/thermal.h>
#include <linux/regmap.h>
#include "lm75.h"


/*
 * This driver handles the LM75 and compatible digital temperature sensors.
 */

enum lm75_type {		/* keep sorted in alphabetical order */
	adt75,
	ds1775,
	ds75,
	ds7505,
	g751,
	lm75,
	lm75a,
	lm75b,
	max6625,
	max6626,
	mcp980x,
	stds75,
	tcn75,
	tmp100,
	tmp101,
	tmp105,
	tmp112,
	tmp175,
	tmp275,
	tmp75,
};

/* Addresses scanned */
static const unsigned short normal_i2c[] = { 0x48, 0x49, 0x4a, 0x4b, 0x4c,
					0x4d, 0x4e, 0x4f, I2C_CLIENT_END };


/* The LM75 registers */
#define LM75_REG_CONF		0x01
static const u8 LM75_REG_TEMP[3] = {
	0x00,		/* input */
	0x03,		/* max */
	0x02,		/* hyst */
};

/* Each client has this additional data */
struct lm75_data {
	struct i2c_client	*client;
	struct device		*hwmon_dev;
	struct thermal_zone_device	*tz;
	struct mutex		update_lock;
	u8			orig_conf;
	u8			resolution;	/* In bits, between 9 and 12 */
	u8			resolution_limits;
	char			valid;		/* !=0 if registers are valid */
	unsigned long		last_updated;	/* In jiffies */
	unsigned long		sample_time;	/* In jiffies */
	s16			temp[3];	/* Register values,
						   0 = input
						   1 = max
						   2 = hyst */
};

static int lm75_read_value(struct i2c_client *client, u8 reg);
static int lm75_write_value(struct i2c_client *client, u8 reg, u16 value);
static struct lm75_data *lm75_update_device(struct device *dev);


/*-----------------------------------------------------------------------*/

static inline long lm75_reg_to_mc(s16 temp, u8 resolution)
{
	return ((temp >> (16 - resolution)) * 1000) >> (resolution - 8);
}

/* sysfs attributes for hwmon */

static int lm75_read_temp(void *dev, long *temp)
{
	
	printk("********lm75_read_temp*******\n");
	struct lm75_data *data = lm75_update_device(dev);

	if (IS_ERR(data))
		return PTR_ERR(data);

	*temp = lm75_reg_to_mc(data->temp[0], data->resolution);

	return 0;
}

static ssize_t show_temp(struct device *dev, struct device_attribute *da,
			 char *buf)
{
	printk("*****************in the show temp*****************\n");
	printk("*****************in the show temp*****************\n");
	struct sensor_device_attribute *attr = to_sensor_dev_attr(da);
	struct lm75_data *data = lm75_update_device(dev);

	if (IS_ERR(data))
		return PTR_ERR(data);

	return sprintf(buf, "%ld\n", lm75_reg_to_mc(data->temp[attr->index],
						    data->resolution));
}

static ssize_t set_temp(struct device *dev, struct device_attribute *da,
			const char *buf, size_t count)
{
	struct sensor_device_attribute *attr = to_sensor_dev_attr(da);
	struct lm75_data *data = dev_get_drvdata(dev);
	struct i2c_client *client = data->client;
	int nr = attr->index;
	long temp;
	int error;
	u8 resolution;

	error = kstrtol(buf, 10, &temp);
	if (error)
		return error;

	/*
	 * Resolution of limit registers is assumed to be the same as the
	 * temperature input register resolution unless given explicitly.
	 */
	if (attr->index && data->resolution_limits)
		resolution = data->resolution_limits;
	else
		resolution = data->resolution;

	mutex_lock(&data->update_lock);
	temp = clamp_val(temp, LM75_TEMP_MIN, LM75_TEMP_MAX);
	data->temp[nr] = DIV_ROUND_CLOSEST(temp  << (resolution - 8),
					   1000) << (16 - resolution);
	lm75_write_value(client, LM75_REG_TEMP[nr], data->temp[nr]);
	mutex_unlock(&data->update_lock);
	return count;
}

static SENSOR_DEVICE_ATTR(temp1_max, S_IWUSR | S_IRUGO,
			show_temp, set_temp, 1);
static SENSOR_DEVICE_ATTR(temp1_max_hyst, S_IWUSR | S_IRUGO,
			show_temp, set_temp, 2);
static SENSOR_DEVICE_ATTR(temp1_input, S_IRUGO, show_temp, NULL, 0);

static struct attribute *lm75_attrs[] = {
	&sensor_dev_attr_temp1_input.dev_attr.attr,
	&sensor_dev_attr_temp1_max.dev_attr.attr,
	&sensor_dev_attr_temp1_max_hyst.dev_attr.attr,

	NULL
};
ATTRIBUTE_GROUPS(lm75);

static const struct thermal_zone_of_device_ops lm75_of_thermal_ops = {
	.get_temp = lm75_read_temp,
};

/*-----------------------------------------------------------------------*/

/* device probe and removal */

static int
lm75_probe(struct i2c_client *client, const struct i2c_device_id *id)
{
	struct device *dev = &client->dev;
	struct lm75_data *data;
	int status;
	u8 set_mask, clr_mask;
	int new;
	enum lm75_type kind = id->driver_data;
	printk("******start probe tmp75******\n");
	if (!i2c_check_functionality(client->adapter,
			I2C_FUNC_SMBUS_BYTE_DATA | I2C_FUNC_SMBUS_WORD_DATA))
		return -EIO;

	data = devm_kzalloc(dev, sizeof(struct lm75_data), GFP_KERNEL);
	if (!data)
		return -ENOMEM;

	data->client = client;
	i2c_set_clientdata(client, data);
	mutex_init(&data->update_lock);

	/* Set to LM75 resolution (9 bits, 1/2 degree C) and range.
	 * Then tweak to be more precise when appropriate.
	 */
	set_mask = 0;
	clr_mask = LM75_SHUTDOWN;		/* continuous conversions */
	printk("in probe switch******\n");
	printk("kind is %d\n", kind);
	switch (kind) {
	case adt75:
		clr_mask |= 1 << 5;		/* not one-shot mode */
		data->resolution = 12;
		data->sample_time = HZ / 8;
		break;
	case ds1775:
	case ds75:
	case stds75:
		clr_mask |= 3 << 5;
		set_mask |= 2 << 5;		/* 11-bit mode */
		data->resolution = 11;
		data->sample_time = HZ;
		break;
	case ds7505:
		set_mask |= 3 << 5;		/* 12-bit mode */
		data->resolution = 12;
		data->sample_time = HZ / 4;
		break;
	case g751:
	case lm75:
	case lm75a:
		data->resolution = 9;
		data->sample_time = HZ / 2;
		break;
	case lm75b:
		data->resolution = 11;
		data->sample_time = HZ / 4;
		break;
	case max6625:
		data->resolution = 9;
		data->sample_time = HZ / 4;
		break;
	case max6626:
		data->resolution = 12;
		data->resolution_limits = 9;
		data->sample_time = HZ / 4;
		break;
	case tcn75:
		data->resolution = 9;
		data->sample_time = HZ / 8;
		break;
	case mcp980x:
		data->resolution_limits = 9;
		/* fall through */
	case tmp100:
	case tmp101:
		set_mask |= 3 << 5;		/* 12-bit mode */
		data->resolution = 12;
		data->sample_time = HZ;
		clr_mask |= 1 << 7;		/* not one-shot mode */
		break;
	case tmp112:
		set_mask |= 3 << 5;		/* 12-bit mode */
		clr_mask |= 1 << 7;		/* not one-shot mode */
		data->resolution = 12;
		data->sample_time = HZ / 4;
		break;
	case tmp105:
	case tmp175:
	case tmp275:
	case tmp75:
		set_mask |= 3 << 5;		/* 12-bit mode */
		clr_mask |= 1 << 7;		/* not one-shot mode */
		data->resolution = 12;
		data->sample_time = HZ / 2;
		printk("choose tmp75\n");
		break;
	}

	/* configure as specified */
	status = lm75_read_value(client, LM75_REG_CONF);
	printk("********probe status is %d\n",status);
	if (status < 0) {
		dev_dbg(dev, "Can't read config? %d\n", status);
		return status;
	}
	data->orig_conf = status;
	new = status & ~clr_mask;
	new |= set_mask;
	if (status != new)
		lm75_write_value(client, LM75_REG_CONF, new);
	dev_dbg(dev, "Config %02x\n", new);
	
	printk("Config 0x%02x\n",new);

	data->hwmon_dev = hwmon_device_register_with_groups(dev, client->name,
							    data, lm75_groups);
	if (IS_ERR(data->hwmon_dev)){
		printk("data->hwmon_dev is error******\n");
		return PTR_ERR(data->hwmon_dev);
	}

	data->tz = thermal_zone_of_sensor_register(data->hwmon_dev, 0, data->hwmon_dev, &lm75_of_thermal_ops);
	printk("data->tz is %d\n",data->tz);
	if (IS_ERR(data->tz)){
		printk("data->tz is error******\n");
		data->tz = NULL;
	}
	printk(dev, "*************%s: sensor '%s'********\n",
		 dev_name(data->hwmon_dev), client->name);

	return 0;
}

static int lm75_remove(struct i2c_client *client)
{
	struct lm75_data *data = i2c_get_clientdata(client);

	thermal_zone_of_sensor_unregister(data->hwmon_dev, data->tz);
	hwmon_device_unregister(data->hwmon_dev);
	lm75_write_value(client, LM75_REG_CONF, data->orig_conf);
	return 0;
}

static const struct i2c_device_id lm75_ids[] = {
	{ "adt75", adt75, },
	{ "ds1775", ds1775, },
	{ "ds75", ds75, },
	{ "ds7505", ds7505, },
	{ "g751", g751, },
	{ "lm75", lm75, },
	{ "lm75a", lm75a, },
	{ "lm75b", lm75b, },
	{ "max6625", max6625, },
	{ "max6626", max6626, },
	{ "mcp980x", mcp980x, },
	{ "stds75", stds75, },
	{ "tcn75", tcn75, },
	{ "tmp100", tmp100, },
	{ "tmp101", tmp101, },
	{ "tmp105", tmp105, },
	{ "tmp112", tmp112, },
	{ "tmp175", tmp175, },
	{ "tmp275", tmp275, },
	{ "tmp75", tmp75, },
	{ /* LIST END */ }
};
MODULE_DEVICE_TABLE(i2c, lm75_ids);

static const struct of_device_id lm75_of_match[] = {

	{
		.compatible = "ti,tmp75",
	},
	{ },
};
MODULE_DEVICE_TABLE(of, lm75_of_match);

#define LM75A_ID 0xA1

/* Return 0 if detection is successful, -ENODEV otherwise */
static int lm75_detect(struct i2c_client *new_client,
		       struct i2c_board_info *info)
{
	struct i2c_adapter *adapter = new_client->adapter;
	int i;
	int conf, hyst, os;
	bool is_lm75a = 0;

	if (!i2c_check_functionality(adapter, I2C_FUNC_SMBUS_BYTE_DATA |
				     I2C_FUNC_SMBUS_WORD_DATA))
		return -ENODEV;

	/*
	 * Now, we do the remaining detection. There is no identification-
	 * dedicated register so we have to rely on several tricks:
	 * unused bits, registers cycling over 8-address boundaries,
	 * addresses 0x04-0x07 returning the last read value.
	 * The cycling+unused addresses combination is not tested,
	 * since it would significantly slow the detection down and would
	 * hardly add any value.
	 *
	 * The National Semiconductor LM75A is different than earlier
	 * LM75s.  It has an ID byte of 0xaX (where X is the chip
	 * revision, with 1 being the only revision in existence) in
	 * register 7, and unused registers return 0xff rather than the
	 * last read value.
	 *
	 * Note that this function only detects the original National
	 * Semiconductor LM75 and the LM75A. Clones from other vendors
	 * aren't detected, on purpose, because they are typically never
	 * found on PC hardware. They are found on embedded designs where
	 * they can be instantiated explicitly so detection is not needed.
	 * The absence of identification registers on all these clones
	 * would make their exhaustive detection very difficult and weak,
	 * and odds are that the driver would bind to unsupported devices.
	 */

	/* Unused bits */
	conf = i2c_smbus_read_byte_data(new_client, 1);
	if (conf & 0xe0)
		return -ENODEV;

	/* First check for LM75A */
	if (i2c_smbus_read_byte_data(new_client, 7) == LM75A_ID) {
		/* LM75A returns 0xff on unused registers so
		   just to be sure we check for that too. */
		if (i2c_smbus_read_byte_data(new_client, 4) != 0xff
		 || i2c_smbus_read_byte_data(new_client, 5) != 0xff
		 || i2c_smbus_read_byte_data(new_client, 6) != 0xff)
			return -ENODEV;
		is_lm75a = 1;
		hyst = i2c_smbus_read_byte_data(new_client, 2);
		os = i2c_smbus_read_byte_data(new_client, 3);
	} else { /* Traditional style LM75 detection */
		/* Unused addresses */
		hyst = i2c_smbus_read_byte_data(new_client, 2);
		if (i2c_smbus_read_byte_data(new_client, 4) != hyst
		 || i2c_smbus_read_byte_data(new_client, 5) != hyst
		 || i2c_smbus_read_byte_data(new_client, 6) != hyst
		 || i2c_smbus_read_byte_data(new_client, 7) != hyst)
			return -ENODEV;
		os = i2c_smbus_read_byte_data(new_client, 3);
		if (i2c_smbus_read_byte_data(new_client, 4) != os
		 || i2c_smbus_read_byte_data(new_client, 5) != os
		 || i2c_smbus_read_byte_data(new_client, 6) != os
		 || i2c_smbus_read_byte_data(new_client, 7) != os)
			return -ENODEV;
	}
	/*
	 * It is very unlikely that this is a LM75 if both
	 * hysteresis and temperature limit registers are 0.
	 */
	if (hyst == 0 && os == 0)
		return -ENODEV;

	/* Addresses cycling */
	for (i = 8; i <= 248; i += 40) {
		if (i2c_smbus_read_byte_data(new_client, i + 1) != conf
		 || i2c_smbus_read_byte_data(new_client, i + 2) != hyst
		 || i2c_smbus_read_byte_data(new_client, i + 3) != os)
			return -ENODEV;
		if (is_lm75a && i2c_smbus_read_byte_data(new_client, i + 7)
				!= LM75A_ID)
			return -ENODEV;
	}

	strlcpy(info->type, is_lm75a ? "lm75a" : "lm75", I2C_NAME_SIZE);

	return 0;
}

#ifdef CONFIG_PM
static int lm75_suspend(struct device *dev)
{
	int status;
	struct i2c_client *client = to_i2c_client(dev);
	status = lm75_read_value(client, LM75_REG_CONF);
	if (status < 0) {
		dev_dbg(&client->dev, "Can't read config? %d\n", status);
		return status;
	}
	status = status | LM75_SHUTDOWN;
	lm75_write_value(client, LM75_REG_CONF, status);
	return 0;
}

static int lm75_resume(struct device *dev)
{
	int status;
	struct i2c_client *client = to_i2c_client(dev);
	status = lm75_read_value(client, LM75_REG_CONF);
	if (status < 0) {
		dev_dbg(&client->dev, "Can't read config? %d\n", status);
		return status;
	}
	status = status & ~LM75_SHUTDOWN;
	lm75_write_value(client, LM75_REG_CONF, status);
	return 0;
}

static const struct dev_pm_ops lm75_dev_pm_ops = {
	.suspend	= lm75_suspend,
	.resume		= lm75_resume,
};
#define LM75_DEV_PM_OPS (&lm75_dev_pm_ops)
#else
#define LM75_DEV_PM_OPS NULL
#endif /* CONFIG_PM */

static struct i2c_driver lm75_driver = {
	.class		= I2C_CLASS_HWMON,
	.driver = {
		.name	= "lm75",
		.of_match_table = of_match_ptr(lm75_of_match),
		.pm	= LM75_DEV_PM_OPS,
	},
	.probe		= lm75_probe,
	.remove		= lm75_remove,
	.id_table	= lm75_ids,
	.detect		= lm75_detect,
	.address_list	= normal_i2c,
};

/*-----------------------------------------------------------------------*/

/* register access */

/*
 * All registers are word-sized, except for the configuration register.
 * LM75 uses a high-byte first convention, which is exactly opposite to
 * the SMBus standard.
 */
static int lm75_read_value(struct i2c_client *client, u8 reg)
{
	printk("********in lm75_read_value\n");
	if (reg == LM75_REG_CONF){
		printk("1\n");
		return i2c_smbus_read_byte_data(client, reg);
	}
	else{
		printk("2\n");
		return i2c_smbus_read_word_swapped(client, reg);
	}
}

static int lm75_write_value(struct i2c_client *client, u8 reg, u16 value)
{
	if (reg == LM75_REG_CONF)
		return i2c_smbus_write_byte_data(client, reg, value);
	else
		return i2c_smbus_write_word_swapped(client, reg, value);
}

static struct lm75_data *lm75_update_device(struct device *dev)
{
	struct lm75_data *data = dev_get_drvdata(dev);
	struct i2c_client *client = data->client;
	struct lm75_data *ret = data;

	mutex_lock(&data->update_lock);

	if (time_after(jiffies, data->last_updated + data->sample_time)
	    || !data->valid) {
		int i;
		dev_dbg(&client->dev, "Starting lm75 update\n");

		for (i = 0; i < ARRAY_SIZE(data->temp); i++) {
			int status;

			status = lm75_read_value(client, LM75_REG_TEMP[i]);
			if (unlikely(status < 0)) {
				dev_dbg(dev,
					"LM75: Failed to read value: reg %d, error %d\n",
					LM75_REG_TEMP[i], status);
				ret = ERR_PTR(status);
				data->valid = 0;
				goto abort;
			}
			data->temp[i] = status;
		}
		data->last_updated = jiffies;
		data->valid = 1;
	}

abort:
	mutex_unlock(&data->update_lock);
	return ret;
}

//module_i2c_driver(lm75_driver);


static int __init lm75_init(void)                                                                                   
{                                 
	printk("**********************add lm75 driver*********************\n");                                                                                    
	return i2c_add_driver(&lm75_driver);                                                                               
}                                                                                                                     
                                                                                                                      
static void __exit lm75_exit(void)                                                                                  
{                                                                                                                     
	i2c_del_driver(&lm75_driver);                                                                                      
}                                                                                                                     
                                                                                                                      
                                                                                                                      
module_init(lm75_init)                                                                                              
module_exit(lm75_exit)




MODULE_AUTHOR("Frodo Looijaard <frodol@dds.nl>");
MODULE_DESCRIPTION("LM75 driver");
MODULE_LICENSE("GPL");

lm75.h