This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1443BOOST: About the output information.

Part Number: IWR1443BOOST

02 01 04 03 06 05 08 07 magic word
04 00 00 01 version?
80 02 00 00 total package length
43 14 0A 00 platform
D4 08 00 00 frame number
8F E0 32 2E cpu cycle time
03 00 00 00 object number
03 00 00 00 01 00 00 00 28 00 00 00 03 00 09 00 02 00 00 00 23 34 E5 FF 20 00 00 00 0D 00 00 00 B1 02 EF FF 10 01 00 00 0D 00 00 00 82 02 09 FF 73 00 00 00 02 00 00 00 00 02 00 00 0C 27 02 2A 77 2B 28 2B 47 29 62 27 22 26 27 24 6C 22 E3 21 22 21 98 21 27 23 DE 23 F1 22 BE 21 E3 1F B0 1F 7B 1E 0D 1E 20 1D D5 1C EE 1C 7A 1D 6E 1D 62 1B 7C 1C 19 1C B8 1C 2A 1D 44 1C 5E 1B 4A 1C C9 1D DB 1D F2 1B 6A 1B A3 1C B8 1C 90 1B DE 1B 08 1D C2 1D 94 1D F5 1C 51 1B C2 1C C0 1D 81 1D 2E 1C 57 1B E8 1A 39 1B 15 1B CD 19 89 1B 3B 1C E0 1B 70 1B DA 1A FF 19 FA 19 D3 1A 33 1B 44 1A 81 19 37 1A A6 1A 6D 1B 68 1A 3E 1A BB 19 D8 18 F4 19 1F 1A B1 19 85 1A 9F 19 CA 19 0F 1A 15 19 87 19 F5 19 03 19 C2 17 27 19 88 18 55 19 A5 19 89 19 B7 18 08 19 08 18 BA 18 3F 19 C5 19 6C 18 16 18 67 18 76 19 0F 1A FF 18 BD 19 F0 19 4C 19 67 18 4B 18 4B 18 B6 18 F2 14 B8 18 A0 18 55 18 43 18 54 17 58 17 BF 17 B0 16 AF 17 8B 18 AA 18 68 18 61 17 88 15 34 17 F3 16 A8 16 31 16 49 17 B0 17 1E 18 32 18 01 17 7C 16 A0 16 BA 16 10 17 A9 16 A6 17 63 17 FB 16 93 16 B5 15 C8 15 D9 16 58 17 08 17 C6 16 0D 17 EF 17 10 18 9A 16 E0 16 22 16 71 16 3A 17 58 17 1E 17 AC 17 3A 17 BE 16 D4 16 50 16 68 15 52 16 01 17 8D 16 9A 16 4B 16 D9 16 A7 16 60 16 5C 16 90 15 F2 16 69 17 08 17 40 16 3B 16 7B 15 20 15 9D 16 9B 16 65 17 0B 17 D7 16 C0 14 40 14 B3 15 D4 15 8C 15 42 10 74 15 2D 15 6F 15 FC 15 77 14 78 14 1A 17 11 17 58 16 45 17 06 14 EF 15 E6 16 C1 16 38 16 75 15 E6 15 FA 15 85 15 8E 13 DD 16 C6 16 D4 16 1F 17 70 17 ED 16 03 16 C7 16 A8 15 30 16 8F 16 12 16 17 16 CA 16 CB 16 B8 15 83 13 6B 16 89 16 60 16 95 15 27 13 40 16 11 16 9A 16 5B 15 F8 12 70 13 26 13 53 15 DF 16 D7 17 47 17 B0 14 82 17 FE 17 D2 18 30 1C 3D 1E 93 1F 55 20 80 21 D5 21 37 22 06 00 00 00 18 00 00 00 9D 07 00 00 0E 1C 00 00 16 26 01 00 00 00 00 00 00 00 00 00 0A 00 00 00 10 00 00 00

hello,

this is the one frame of the output information(out-of-box demo), I could just understand the header information, but for the rest, I don't konw how to analyze. Could you give an detailed explanation? 

  • Hello,

    Please check the following thread where a few ways to interpret the data sent over the UART port for mmWave Demo is discussed:

    IWR1443: Get data from mmWave Demo GUI

    Hope that helps. Please let us know if you have further questions.

    Thank you,

    Vaibhav

  • Hi,

    If you double click on C:/ti/mmwave_sdk_01_00_00_05/packages/ti/demo/xwr16xx/mmw/docs/doxygen/html/index.html and scroll down to "Output information sent to host", you can see the structures that are output to the port. 

    Keep in mind, the data structure will vary slightly depending on what  parameters are enabled in the guiMonitor section of the cfg. That is, certain fields of data will enabled/disabled according to the cfg. The possible data fields that can be sent are:

    • Detected objects
    • Log magnitude range/range profile
    • Noise floor profile
    • Range-azimuth heatmap
    • Range-doppler heatmap
    • Stats information

     You can verify which data fields are enabled by looking at the "Console Messages" on the Visualizer and looking at the line that starts with guiMonitor. Section 3.5 of the "mmWave SDK User Guide," which can be found in the docs folder of the SDK installation, goes into detail about which parameter belongs to which data field.

    You can also reference the following file in the mmWave SDK installation(search for the MmwDemo_transmitProcessedOutput function):

    file:///C:/ti/mmwave_sdk_01_00_00_05/packages/ti/demo/xwr14xx/mmw/docs/doxygen/html/main_8c.html#ac3a90335aea273ffb5d4cc76d780a55d

    Please let me know if this answers your question or if you need further clarification.

    Regards,
    Kevin

  • Closing due to inactivity. If you have additional questions, please start a new thread.