Other Parts Discussed in Thread: UNIFLASH, SYSBIOS
Tool/software: Code Composer Studio
We are using the AWR1642 development platform and have been able to compile and run the MMWave demo source under Debug Mode (per the document "xWR16xx_mmw_user_guide.pdf" that came with the SDK). We are running that source on the board through CCSv7 on a PC.
For reference, I am looking at section 4.1 "Preparing the EVM".
However, we would also like to run things in "Deployment Mode" by flashing the binaries to the board so that we can run without CCS or the PC.
But when we use the Uniflash tool to program the .bin that has been created by CCS onto our development board so that it can run standalone from the PC, we are unable to establish communication with the development board, as though the board had not been programmed properly.
What is the proper procedure for Deployment Mode, to program the QSPI with a .bin that has been built in CCS?
Thanks in advance,
Joe Shidle