This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

FDC2214: To certify IEC61508

Part Number: FDC2214


To whom it may concern.


Our customer is considering FDC2214 and their end equipment will be needed IEC61508.

FDC2214 has core which is drawn in the simplified schematic of datasheet.

They inquired TUV to certify IEC61508 and TUV said FDC2214's core must be designed by following IEC61508-2 Annex F.

Was the core designed by IEC61508-2 Annex F?
If yes, Could you provide any evidence?

Your reply would be appreciated.
Thanks and best regards.