This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDC1000-TDC7200EVM: TDC1000-TDC7200EVM

Part Number: TDC1000-TDC7200EVM

dear sir

iam interfacing a TDC1000-TDC 7200 EVM board to the lpc 1769 controller for flow meter application .

iam facing one major problem.

which is

i got a responce from the sensor but the time of flight value  is not varied based on flow rate it shows only 1 t0 15 nano seconds time of flight value even we are applying 120 to 140  nano seconds time flight value.

is there any wrong in my configuration please provide configuration values?

my configuration are

 TDC1000(analog front end device) configurations 

CONFIG0    0x45

CONFIG1   0x45
CONFIG2    0x12
CONFIG3    0x01
CONFIG4    0x1f
TOF1          0xc8 
TOF0          0x1e
 ERR_FLAGS  0x03
 TIME_OUT     0x19
 CLK_RATE     0x01

TDC7200(stop watch timer) configurations are

CONFIG1                           0x83
 CONFIG2                          0x44
 INT_STATUS                     0x1f
 INT_MASK                          0x07
 COARSE_CNTR_OVF_H          0xFF
 COARSE_CNTR_OVF_L           0xFF
 CLOCK_CNTR_OVF_H             0xFF
 CLOCK_CNTR_OVF_L              0xFF
 CLOCK_CNTR_STOP_MASK_H     0x00
 CLOCK_CNTR_STOP_MASK_L      0x00

if it is any wrong in configuration please provide accurate configuration values

regards