Hello everyone,
We have been using the mmwave radar for a few weeks now by mounting it on the front of our development vehicle. Although we have been able to figure out the basic operation of the radar we still have doubts about the detection process as the outputs which we get are many times inconsistent.The details of the configurations are also attached below :
I have the following questions depending on a few scenarios :
1. While testing for Adaptive Cruise Control, most of the time we start detecting the vehicle in the front at around 35-40 meters (Max unambiguous range is 50 m). Despite driving in a straight path following the vehicle we see that the detection is sometimes lost in between and gained back again. There have been cases where we have seen the detection being lost even in close distances around 10 m or so. Also, many times the vehicle is not detected at all. What could be reason for such non uniform outputs ?
2. After some reading we discovered that the maximum Doppler velocity is 30 kmph(approx 18 mph). Now we have major problems when we try moving towards a stationary vehicle. Could this maximum Doppler velocity be causing problems that cause us lose detection ? Because we have also experienced that we detect objects quickly and steadily at lower speeds ( around 15 mph) and detection becomes poor at a bit higher speeds ( around 25 mph) in case of running into other stationary vehicle.
3. One of our observations is that we get many detection points when the vehicle moves under a bridge. Is it a drawback for the radar ? If yes then do you suggest some remedies for it ? Also are there any other such factors which affect the radar output ?
4. Sometimes we have also observed that we get many noisy detection points when we move through the areas where we have many objects around ( driving through intersections, across buildings etc ). What can be done to eliminate this ?
5. So far the only method to set configuration parameters on the radar we know is of using the visualizer. We also calculated some values using the estimator and made changes in the parameters like profilecfg, chirpcfg and it helped us improve our outputs. However, is there any other way we could set/ change the parameters ? Because for example we only have maximum range of 50m allowed on the visualizer where as we can use the radar with max range of 80 which could be really helpful for ACC. In your own testing do you have some parameter values for ACC which you would like to share ?
Thanks.