Hello,
I run the Solution Software GUI v1.9.2 on a Windows 7 - 64Bit System.
- When connecting the LDC1101EVM-Board to my System the green LED on the EVM-Board lights but nothing happens. The GUI shows in the bottom left corner "Not connected"
- When connecting the LDC1000EVM-Board to my System the board is recognised and everything works.
In case 2 the Devicemanager of my Windowssystems shows a EVM at a COM-port, in case 1 (when connecting the LDC1101EVM) not.
Do I need an additional device Driver or did I something wrong.
Thanks,
Frank