Hi,
I am going to apply a calibration code which will first work on AFE4405EVM board and then will be implemented on my own embedded board. I have questions regarding duty cycle:
1. Does the calibration code(included in the AFE4405EVM FW) work by controlling only the TX current and RX resistance(Rf) ? Or does it change also duty cycle ?
2. The EVM default value of the duty cycle is 1% at 100Hz sampling rate. It seems that the maximum value of the duty cycle is 10% for 100Hz sampling rate and the maximum of duty cycle increases when sampling rate is higher, say 500Hz. My question is : what is good value of duty cycle for 80Hz ~ 100Hz ? Is 1% good candidate as it is the default ? How about 3% ~ 5% ?
Regards,
Konan