This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1443: COM port can't work ok in Linux PC

Part Number: IWR1443


Hi,

My customer's IWR1443 board works ok in windows PC and now they wants to move the Linux PC.

They installed the CCS7.2 in ubuntu14.04 and the CCS works ok with the board. They saw ttyACM0 and ttyACM1 in /dev, but when they tried to connect with ttyACM0, they can't get right respond.

I tried Ubuntu 14.04 64-bit in VMware with the IWR1443 EVM and the com ports work ok. I can't reproduce the problem.

Do you have any idea/comment on the com port issue in Linux PC?