This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1443BOOST: Access to auxiliary data port based on Tera Term

Expert 1985 points
Part Number: IWR1443BOOST


Hello,

IWR1443Boost started to work, but why is the output data is wrong?

Auxiliary data port (COM4)-baudrate:921600

User UART (COM3)-baudrate:115200

Thanks and best regards,

Amin

  • Hello Amin,

    What kind of info are you seeing in the actual GUI? Once you have the demo running through the terminal, you should be able to view the data through the mmWave Demo GUI. Are you seeing any valid data in the GUI? Also, have you tried loading the profile config directly through the GUI?

    Regards,

    Adrian

  • Hello Adrian,

    Based on "Serial Port Utility"problem solved.
    The format of output data must be HEX .

    Thank you.

    Best regards,
    Amin