Other Parts Discussed in Thread: UNIFLASH
Tool/software: Code Composer Studio
Hello everyone
I am using CCS 7.1.0 to connect with AWR1642BOOST and load the custom project. So, I close the jumper SOP0 and SOP1. The target configuration file I used is in the attachment. When I was trying to connect with the device, it pops out an error said that:"Cortex_R4_0: Error connecting to the target: (Error -2062 @ 0x0) Unable to halt device. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 6.0.628.1) "
BTW, I can run the demo. i can connect with device in "function mode" with closed jumper SOP0.
Can you tell me how to solve this problem?
Thanks
Xining