This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1443: In this, can I take ADC data directly from adc buffer in any form like LVDS?

Part Number: AWR1443
Other Parts Discussed in Thread: MMWAVE-SDK, MMWAVE-DFP

Hi,

I want to read LVDS ADC data directly from the ADC buffer, from external FPGA. Is there a way to do it? and at what speed can I collect that LVDS ADC data?

Thanks,

Vinayak

  • Hello Vinayak,

    You can use the "Capture Demo for xWR14xx" CLI based application in the MMWAVE-SDK to get the ADC data over the LVDS to external FPGA . The data format and the data rate can be configured and passed as the configuration script to CLI window.
    For more information on how to configure and use the capture demo please refer to "Capture Demo for xWR14xx" in the MMWAVE-SDK User Guide.

    You can also configure the device to give LVDS data using the RadarStudio which is part of the MMWAVE-DFP.
    Please refer to "Section 5 Radar API Tab Operations" in the "RadarStudio_User's_Guide.pdf" on how to use and configure the device using RadarStudio.

    Thanks,
    Raghu