This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE5818: AFE5818 LVDS differential routing pin delay / internal wiring length

Part Number: AFE5818


Dear Sir/Madam,

Fig 108, top layer routing showing that LVDS data and ADC clock has delay between P and N pins.

For example LVDS serialized differential data outputs for channel 4 has two pins: U13 (DOUTM4) and T13 (DOUTP4). On the figure the trace for T13 is longer compared to the trace for U13. I assume that the pin U13 has internal delay vs. pin T13 equal to 289NFBGA pin pitch = 0.8mm.

Can you please confirm that information and provide a table with delay length (internal wiring length) for all differential interface pins?

Best Regards, Vassili