Hi,
I would like to use the TMP108 for temperature sensing in an application, where I need high relative accuracy. I am doing a calibration in the beginning, so the absolute accuracy is not the point.
The absolute temperature accuracy of ±0.75°C (max) from –20°C to +85°C specified in the data sheet . The relative accuracy should be much smaller.
Could anyone provide data on the hysteresis behavior of this device or the long term stability?
Thank you
Best Regards
Doris